Other Parts Discussed in Thread: SE555
Hello,
I need a timer capable of accurate timing to 3 months (= 90days = 7,776,000s), at which time it will then trigger an external event through a FET (or similar). The timing will begin when the timer senses a loss of main power. The 3 month timing duration will then be ran off battery power. In addition to this, the timer needs reset capability and manual override input. The manual override will be provided to the timer via a signal processed by a RF chip.
I am looking for accuracy, simplicity, reliability, low power consumption, and hopefully an internal frequency generation.
I am considering a few options and need help sorting them out.
Option 1: Timer combined with a counter/comparator
Option 2: Clock combined with a comparator
Option 3: MCU
Are there TI products that can be provided for each of the above options? Are there other, better, options?
Thanks!!!