This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE72010 configuration through SPI interface

Other Parts Discussed in Thread: CDCE72010, ADS62P49

Hello to all,

My professor asked me to do a reference design using TI's TSW4200 AD/DA EVM kit and Xilinx ML605 EVM board. The reference design is to design a Dightal up-converter and a digital down-converter on Xilinx's FPGA and create a data loop with TSW4200 AD/DA EVM boards.

According to the design, I need to use cdce72010 on TSW4200ADC EVM board to generate a 61.44MHz clock for ADS62P49. I use onboard 491.52MHz VCXO and a 19.2MHz external reference clock from TSW4200DAC EVM board. And I plan to implement a SPI interface between TSW4200ADC EVM board and ML605 board to configure the cdce72010. But after several tries I just can not get the required clock from cdce72010. The clock generated by cdce72010 is always 245.76MHz. 

The cdce72010's registers value are shown below (from register0 to register12):

683C0050, 68000021, 83040002, 68000003, E9800004, 68000005, 68000006, 83800017, 68000098, 68050CC9, 0C000F0A, 0000040B, 0000180C

Since I'm new to this area, any advices are welcomed.

 

Thank you,

Xuming Zhou