Other Parts Discussed in Thread: USB2ANY, LMK03318, LMK03806
Hi there,
I am currently evaluating LMK03806B clock module using LMK03806BEval.
I am able to program the EVM using USB2Any (although there are issues with the direct connectivity of uWire pins, I got it working with the help of this thread) and TICS Pro GUI.
I am seeing the correct CLKout (Freq & output format) as I program.
1. However, the PLL is not getting locked to the onboard crystal (100 MHz crystal on the EVM).
Please see the below snippets of my current configuration:
a) USB2ANY & EVM connectivity (as per this thread)

b) User controls (NO_SYNC's are checked because SYNC cable is not connected between USB2ANY & the EVM)

c) PLL settings

d) CLK outs (enabled only CLKout2)

2. Secondly, my application requires 491.52 MHz CLK. I am hoping to use the onboard 100MHz Crystal (of the EVM) to achieve this Clk freq (491.52 MHz). I am not able to program the VCO freq and other parameters (PLL_N, PLL_R, PDF etc.,) that can yield this freq (if at all it is possible?)
Could anyone please help me with the above two queries?
Many thanks
Hima