This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK05318BEVM: brand new LMK05318BEVM appears to be dead on arrival

Part Number: LMK05318BEVM

HI I was having problems with an older TI eval board so I purchased a new LMK05318BEVM. Jumpers are set up as per the manual and the IIC is able to find the part but there is no output. The supply current is 220mA and when I load new code there is some form of output during load but goes away after loading is complete. What I need to be able to do is demonstrate a 400MHz output with a 25MHz reference input. Any ideas, or do I have a bad board ? Best Steve