Part Number: LMK03318
Hi,
In the datasheet there are IDDO values for VDDO_01, 23, 4, 5, 6, and 7.
Later in the datasheet it is stated that if any of outputs 4-7 are disabled then their corresponding VDDO can be connected to GND.
Does this rule apply to outputs 01 and 23? That is, if outputs 2&3 are disabled can you connect VDDO_23 to GND?
If however, VDDO_23 has power applied but the outputs 2&3 are disabled, is IDDO_23 0mA or the value stated (85mA typ)?