Part Number: LMK05318B
Can the clock output be configured to at least 10dbm power?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK05318B
Can the clock output be configured to at least 10dbm power?
Hi
I have a LMK05318B Evaluation board and I did some measurements:
I'm using 32MHz LVCMOS type output at 50ohm load, and the output level is between +6 to +6.5dBm (for the 1st 32MHz harmonic only)
I also measured the entire signal bandwidth using a power meter, the signal power is about +9dBm at 50ohm load.
If you require at least +10dBm and your output load is 50ohm, I'm not sure it is possible.
If your output impedance is high, I think you'll be ok but the output will no longer be 50ohm matched and you will need to keep it very short in order to avoid reflections.
Nir
Hi Mien,
Per Nir's comments, 10 dBm power cannot be guaranteed. The maximum output swing is spec'ed in the datasheet as follows:

Regards,
Jennifer