Part Number: TLC555
Hi Team,
We want to use the TLC555 timer as a sequence controller.
After the IC main power rail rises and de-asserts the reset signal with a delay of 60-80ms .
Is it doable?
Thanks
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jimmy,
Can you provide more information or illustrate what the customer is looking for? I am unclear based on the description. My interpretation is that the main power rail will control the reset pin. I am unsure of the delay function in the description above. A more descriptive explanation of the desired input, output and supply signals would help me better assist. For example, is the main ic power rail also powering the timer? Are you looking for a delay from the time reset is de-asserted and the output signal changes? Etc.
The power supply needs to be fully on to at least minimum supply prior to the reset pin control being recognized by the device.
Best Regards,
Chris Featherstone