Part Number: LMX2594
Other Parts Discussed in Thread: TIDA-01021, LMK04828, ADC12DJ3200
Hi,
I have a question about alignment of sysref clock for two LMX2594 which need to realize multi-chip synchronization . My setup is listed below figure1 shown:
- OSCIN of two lmx2594 are provided 100MHz reference clock from very-low skew clock buffer
- SYSREFREQ of two lmx2594 are held high so as to work at "Master -Continuos" mode
- RFAout of two lmx2594 output 10GHz RF clock
- RFBout of two lmx2594 is selected to Sysref Clock which output 4.8828125MHz clock for JESD204B
As below figure2 shown, LMX2594 will work at Category1 for RFAout, that means the 10GHz RFAout will align with 100MHz OSCIN. Figure3 show that alignment of 100MHz OSCIN between two lmx2594. So the RFAout of two lmx2594 will align with each other if the 100MHz OSCIN of two lmx2594 will align with each other at the Pin location. But, the sysref clock of two lmk2594 don't align with each other as below figure4 shown.
How could I align sysref clock between LMX2594 when need to realize multi-chip synchronization?
Or, programming the JESD_DAC1_CTRL, JESD_DAC2_CTRL, JESD_DAC3_CTRL, and JESD_DAC4_CTRL words to realize alignment as figure5 shown?

Figure1

Figure2

Figure3

Figure4

Figure5
Best regards!!!
Jason