This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM7005: LVPECL VOD maximum specification

Part Number: CDCM7005

Hi Team,

My customer is considering to reuse their previous CDCM7005 design into new project and urgently requesting to check the information below.

- What is LVPECL VOD max specification? Datasheet only specifies min spec 500mV. 

- When calculating with VOH and VOL, its min value should be 0.37V (VCC-1.55-VCC+1.18) and its max value should be 1.19V (VCC-2-VCC+0.81), which are not corresponding to VOD spec 500mV. 

Thank you for your support.