This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595EVM: Deterministic Phase between the OSCin and RFout pin

Part Number: LMX2595EVM
Other Parts Discussed in Thread: LMX2595

Hi, 

Here i am using the LMX2595 in Category 3 and Ref Osc frequency is with in the limits. I gave SYNC s/g (1MHz)from the external pulse generator but could not see deterministic phase . Can any one clarify my below questions

1. In data sheet , it is mentioned that it is time critical. How can i achieve that ? (Would like to check in Lab)

2. In The phase synchronization reference design , what is the procedure to setup Timing critical example?

https://www.ti.com/lit/ug/tidud11/tidud11.pdf?ts=1668028477124&ref_url=https%253A%252F%252Fwww.google.com%252F

Thanks