Part Number: LMX2491
Hi,
I am trying to analyze the phase noise of the entire PLL when External VCO and Loop Filter is used and i have following queries:
1)According to theory, the phase noise of PLL will follow the OCXO (Reference Oscillator) Noise within loop bandwidth. But i am not able to see the result when i simulate LMX2491.
2) According to theoretical calculation the OCXO (100MHz), have phase noise of -155dBc/Hz @ 1KHz offset; I want to understand why PLL phase noise is not improving beyond -97dBc/Hz at 1KHz offset.
3) I am not able to load the OCXO and VCO phase noise data as the error says "Offset violates 3 point model assumption" and "The 1/f^3 noise could not be calculated".
Kindly guide me to evaluate the correctness of the design



(this is not the correct config)