Part Number: LMX2487
Hi team, working with a customer on this device. LMX248.
The datasheet indicates that the device doesn’t necessarily require differential operation on the FinRF pins, and in fact can be run single ended if you shunt the complementary input with a capacitor. However it is unclear if the input power sensitivity changes if you run it in single ended mode vs. differential mode. Does the max/min input sensitivity change in single ended operation? And if so, what does it change to?