Part Number: LMK05318
Hi :
Datasheet, power consumption example, page 75:
1) Why there is 70mA in power consumption calculation in page 75 of datasheet, for every output?
IDDO_01 = 70 + 16 + 16 = 102 mA
• IDDO_23 = 70 + 14 + 14 = 98 mA
• IDDO_4 = 70 + 10 = 80 mA
• IDDO_5 = 0 mA
• IDDO_6 = 70 + 25 = 95 mA
• IDDO_7 = 70 + 6 = 76 mA
2) If all output frequencies are the same, same divider scale, how 70mA would change in above datasheet example?
3) Is there a SW tool by TI to estimate power consumption of LMK05318, based on design settings ?
Thanks,
K.