This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04828: Clock output is not what I set.

Part Number: LMK04828

Hi,

I set lmk04828 single loop 0-delay and changed FB_MUX_EN ald PLL2_NCLK_MUX as same value as Table 8 of datasheet.

The OSCin was 288MHz and VCO was selected as 2592MHz.

I expected 288MHz on DCLKout(Clock Divider = 9) 9MHz SDCLKout(SYSREF Divider = 288)

However, the output of DCLKout was about 296MHz and SDCLKout was about 9.26MHz

What should I do get proper output?

 I attached tcs file and screen capture files.

LMK04828_oscin_single-loop_2022_1121_sysref.tcs

Regards,

YS