Part Number: LMX2594
Other Parts Discussed in Thread: LMK00304, LMX2572EVM
Hi,
As the datasheet don't describe clearly, I have three questions about Category for SYNC mode and MASH_SEED function as below figure shown:
1. What difference is between the two Category1 marked red and blue circle?
2. In the Category1 marked red circle,
Is "SYNC Mode Required" meaning that VCO_PHASE_SYNC must be set as 1?
Is "No Software/Pin SYNC Pulse required" meaning that not need SYNC input and not need toggling VCO_PHASE_SYNC bit? " If yes, how to trig SYNC action?
3. As I know, the part of Channel divider is included as the IncludeDivider when SYNC Mode is enable. IncludeDivider will be in the loop, and has deterministic delay.
so the CHDIV in the judgment box as below figure shown is the rest of Channel divider which exclude the IncludeDivider part, right?
4. when MASH_ORDER is 0 that means it work as integer mode, Phase Adjust function by programming MASH_SEED value could be work?

Best regards!
Jason