Part Number: LMK04828
Hi, all:
I read the multi-clock SYNC app note(Multi-Clock Synchronization) carefully, which is suggested by Ajeet Pal. There is a question about case 2 of ZDM example:
As below figure.1 shown, when R' is not 1, it will bring phase uncertainty from input to output. In case 2 of ZDM example, reference frequency(60MHz) and output frequency(40MHz) are not integral multiple relation

figure.1
As below figure.2 shown, if I change condition as following, I got N' / R' = 5 / 2 at last. So R' is not 1, which will bring phase uncertainty according to case 2. But reference frequency(60MHz) and output frequency(30MHz) are integral multiple relation(twice), So, question is if Integral multiple relation will align edge of reference frequency and output frequency? if yes, does it cause phase certainty?
Reference frequency = 60 MHz, VCO frequency = 150 MHz , Output frequency = 30 MHz, D=5, N=3

figure.2
Thanks in advance!
Best regards!!!
Jason