This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2430: Questions about the LMX2430_Simulator

Guru 12065 points
Part Number: LMX2430

Hi, 

Is it possible to check the modulation characteristics (VCO modulation)?

For reference, I attach a characteristic graph displayed by ADI's ADIsimPLL.

Is it possible to display such a graph in [PLLatinum Sim] as well?

Thanks,

Astro

  • Hello Astro,

    PLLatinum Sim does not have the phase shift curve as shown in the figure above, however, it does have the amplitude curve. To obtain it:

    - Select your device in the start page under (1) "Select Device" tab, then (2) select "LMX2430," and finally (3) click on "Load Device" button:

    - Click on (1) "Bode Plot" tab and then on the (2) advanced option on the left to obtain the VCO gain curve:

    Hope this helps!

    Good Luck,

    Andrea