Part Number: CDCBT1001
Other Parts Discussed in Thread: CDC3RL02
hi team:
my customer have a use case and want to check whether the CDCBT1001 is suitable for this case as below green mark area. Can you help to confirm? tks !
here attached the parameter and block diagram:
1. signal input is a 0.1~ 0.6V(Vpp), typical is 0.4V, Sinusoidal signal with10Mhz
2. the final signal will go into STuw81300 CLK device, and the input signal has the following requirements.
3. Reference phase noise -155dBc@10kHz offset.