Part Number: CDCEL9XXPROGEVM
Other Parts Discussed in Thread: CDCE937, CLOCKPRO
Hi,
I have a CDCEL9XXPROGEVM evaluation board as I want to tweak some setting in a CDCE937 device.
However, I cannot connect to the board when running the clock pro wizard and development tool part, never see a green circle all refreshes just bring up local options. The stage thing is if I go into the "Programming EVM Tool" and select the device the development board is found and I can connect (see image). However, going into the other options that eventually launch the "TI Clock Pro 1.2.1" window which would all me to with the option to adjust setting the device/eval board are not found I only ever get a local option. How do I make Clock Pro find the board/Chip?
I am currently running on Windows XP as it did work at all on my current Windows 10 machine.