Part Number: LMX2595
Hi,
in the datasheet of the LMX2595 you recommend the following power-up sequence:
1. Apply power to device.
2. Program RESET = 1 to reset registers.
3. Program RESET = 0 to remove reset.
4. Program registers as shown in the register map in REVERSE order from highest to lowest.
5. Wait 10 ms.
6. Program register R0 one additional time with FCAL_EN = 1 to ensure that the VCO calibration runs from a stable state.
I have a few questions regarding that procedure:
Does the 10ms waiting time relate to point 1 or point 4 in the power-up sequence and whats the reason for this waiting time?
Is it possible to start the VCO calibration when the CE pin is low?
Kind regards
Christian