This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: 6.4 GHz pulse with SYSREF

Part Number: LMX2595


I would like to use SYSREF to produce a series of pulses at 6.4 GHz with some phase delay. 

Looking at the table for the SYSREF set up on page 37 of the LMX2595 spec sheet, it says that the maximum value of f_interpolate is 1.5 GHz. From here f_interpolate passes through SYSREF_DIV and then is divided by 1/2. 

Does this mean that the LMX2595 frequency synthesiser can't generate a series of pulses at 6.4 GHz with a programable phase delay? 

If this is the case, any recommendations on a frequency synthesiser that meets these requirements would be greatly appreciated.