Other Parts Discussed in Thread: LMK04832
Hi Ti Team,
We are using Evm of LMK04832 and could not able to get the output frequency 122.88 at CLKout pins when onboard 122.88MHz cystal is used ( LMK is used as distribution network and Plls are disabled) . please see the attached configuration fileLMK_122.88MHz onboard VCXO.tcs.
kindly let me know what am i missing?
FYI: 1)observed 122.88MHz signal at input of LMK (43 and 44pins).
2)observed all outputs if i have given external signal to CLKin1 (used as distributed Network/Plls are disabled) but not by using on board 122.88MHz onboard VCXO