Part Number: LMK04828
Hi,
We are using LMK04828 clock synthesizer. Please find the attached schematic snapshot along with the tics pro clock file we're using.
1) We're unable to get following o/p clocks. Even though it looks like it's enabled in GUI.
SDCLKOUT1_P 7.68 MHz
SDCLKOUT5_P 7.68MHz
SDCLKOUT3_P/SDCLKOUT3_N 7.68MHz
2) Also we couldn't configure all the required clocks. Our requirement is as follows:-
DCLKOUT0_P/DCLKOUT0_N 245.76 MHz
SDCLKOUT1_P 7.68 MHz
DCLKOUT4_P/DCLKOUT4_N 245.76 MHz
SDCLKOUT5_P 7.68 MHz
DCLKOUT8_P/DCLKOUT8_N 100 MHz
SDCLKOUT9_P/SDCLKOUT9_N 27 MHz
DCLKOUT10_P/DCLKOUT10_N 52 MHz
SDCLKOUT11_P/SDCLKOUT11_N 125 MHz
SDCLKOUT3_P/SDCLKOUT3_N 7.68MHz
LMK04828_156.25MCLKin0_122.88MVCXO_245.76MDCLK_7.68MSYSREF.zip