Hello,
For our design we need to provide 1.3GHz clock output (and further divider frequencies of 1.3GHz).
Therefore I set up our LMK04832EVM to single loop mode with 130MHz reference input and PLL2 settings to tune VCO0 to 2600MHz.
TicsPro shows the frequency in red because it is 20MHz out of its specified range (max 2580MHz).

In my test setup this seems to run stable. I did not recognised any problems also in longer test series.
Is the specified range of 2440 - 2580MHz a hard limit where problems are known when operating ouside of this range. Or is this just a range where the VCO is qualified and the proper operation can be guaranteed?
Are there any test results of operating the VCO outside this range or known issues that might occur?
Regards,
Hendrik