Part Number: LMK03328
Hi Team TI,
We are using LMK03328 in Hard Pin Mode(ROM Mode). We want to load the below default configuration as default.

Our O/P clock requirement = 100MHz LVCMOS clock single ended ( its default on OUT4).
Input we have as below,
Clock input = 100MHz, PRI_P.
do we need to change it?
Let us know, what is primary or secondary clock requirement for above configuration to load?
Also can we change it in SW Pin mode if we use above configuration?