Part Number: LMK03318
HI,
This is related to prev case CS1525439
1. For ROM mode, the GPIO[5:0] = 24d = 0b011000, what is the value for REFSEL (2state)? The document stated REFSEL Vim =0.9V for SEFREF selection for 3state. How about 2 state ?
I am using a XO connected to SECREF.
- SECREF_P/N = 50MHz XO(7M50072001))
- GPIO5 = Low
- GPIO4 = High
- GPIO3 = High
- GPIO2 = Low
- GPIO1 = Low
- GPIO0 = Low
- HW_SW_CTRL = High
- REFSEL = 0.9V ?? (Input mid voltage for the 3-level logic, this selects the secondary clock as the PLL preference)
- PDN - connected to gnd via a 10nF

2. Can u verify if the above setting connection below can work when pwr on ? Expect when power on, auto generate diff clk output (OUTPUT0,1,2,3 = 156.25Mhz, LVDS, OUTPUT4,5 = 100MHz, LVDS). Any additional setting needed ?

rdgs
stloh