hello sir.
You want to enter it into LVCMOS_CLK of LMK00804B using 40MHz TCXO. For VDD and VDDO on the LMK, enter 3.3V.
My TCXO output range is 0.8Vp_p.
If you look at the datasheet, the VIL of LMK00804B is max 1.3V and VIH is min 2V, so it should not work.
However, the output has been confirmed to swing at 3V. I don't understand why you're doing this.
Please explain.
thanks
mr.lee