Other Parts Discussed in Thread: CDCE913
Hi Expert,
I have CDCE913 IC, configure through i2C.
I am able to get desired output frequency but my amplitude and pick to pick voltage is changing when i am changing the frequency. Is it like that only or something is wrong. PFA image for reference.
- Default 25MHz frequency
- 50Mhz frequency with the following setting
- M=4
- N==40
- Fin=25Mhz
- Fvc0=250Mhz
- Pdiv=5
- P=1
- Q=20
- R=0

- configuration register is
- output selection Y1_7,FS1_7,SSC1_7 and Y2Y3_7
- Y1_ST1 = 01, Y1_ST0 = 11
- XCSEL = 0x09
- SSC1_7 = 0b0111 / 0b001
- Y2Y3_ST1=01, Y2Y3_ST0=11
- SSC1DC = 0/1
- VCO1_0_RANGE = 11 >175MHz
- VCO1_1_RANGE = 11 >175MHz
Please help me out.
Waiting for your feedback.
--
Thanks & Regards,
Divyesh Patel