Part Number: LMX2572
Other Parts Discussed in Thread: LMX2571
Hello
We are trying to use the full assist programming mode on the LMX2572 PLL chip. We have built up the look up table of the values of VCO_SEL, VCO_CAPCTRL and VCO_DACISET over the VCO range 3.2 to 6.2 GHz.
Then, we program REG20, REG19 and REG16 with values from the look up table. We then program registers 75, 45, 44, 43, 42, 37, 36, 34, and 14.
When testing the prototype we are finding that we need to complete the programming sequence by writing to Register 0. If we do not write to Reg 0, the chip does not program. Is this what is expected?
The other issue is that we are finding odd frequencies which do not achieve lock. Even some frequency values that fall precisely on a look up table value do not achieve lock.
Any comments regarding what the programming sequence should be or any tips in getting the fully assisted mode to work will be welcomed.