Part Number: LMX2592
When selecting the "Default Configuration" menu item are the register values that are loaded supposed to be recommended values as a starting point, or are they supposed to match what the datasheet indicates as default values? We are seeing discrepancies with some of the values and it's not clear whether this is an error or intentional. Specifically:
Reg0, CAL_CLK_DIV: Datasheet says 3 is the default, but TICSPRO uses 0
Reg13, CP_ICOARSE: Datasheet says 1 is the default, but TICSPRO uses 0
Reg35, CHDIV_SEG1_EN: Datasheet says 0 is the default, but TICSPRO uses 1
Reg47, OUTB_POW: Datasheet says 0 is the default, but TICSPRO uses 15
Reg64, FJUMP_SIZE: Datasheet says 15 is the default, but TICSPRO uses 7
We are using rev F of the datasheet and v1.7.5.7 of TICSPRO