Part Number: LMK05318
Other Parts Discussed in Thread: LMK05028, , LMK03318, LMK5B12204, LMK03328, CDCE6214
I was told that the LMK05028 require two input oscillators, that is one too many.
It also requires the second oscillator connected at the XO pin to be in a 48...54MHz frequency range.
I cannot find any purchasable oscillator in that range that also provides <0.3ps RMS jitter. There are parts with 1...3ps jitter, but those are not usable in my application.
156.25M oscillators are readily available with <0.3ps jitter from multiple vendors.
So, is there any LMK clock chip that can run from a single 156.25MHz oscillator, have low jitter, EERPROM and fractional PLL?
Any of these can operate with XO disconnected? LMK05318, LMK03318, LMK5B12204...