I have a master LMK04828 that drives a slave LMK04828.
The slave device acts as a buffer and is used to expand the number of JESD REFCLKs and SYSREFs.
I want to connect the master's SDCLKout1+/- to drive the slave's CLKin0+/- as a JESD SYSREF DC-coupled differential LVDS signal.
(SYSREF is a pulsed signal so it must be DC-coupled, not AC-coupled.)
The master's DCLKout0+/- drives the slave's CLKin1+/- as the JESD REFCLK; this can be AC-coupled since it's a clock.
I don't see specs in the datasheet specifying VICM_DC (input common mode voltage for DC-coupling) and VIDIFF (differential input voltage min and max) for the CLKin0+/- input.
Are these specs available? Can I DC-couple the two devices for a non-periodic SYSREF?