This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TICS Pro

Regarding TICS Pro.
After setting Post R to "2" (Fig.2) from the state of Fig.1, the value of Fraction seems to be wrong.
I think "1/40" is correct for Fnum/Fden.
Since the software version (V1.6.10.0) is old, is it not the correct value?
(Do I have to enter it manually?)

Regards,
Akihiko Yokouchi/

 Fig.1

 Fig.2