Part Number: LMH1983
Dear Technical Support Team,
There is following VCXO on my board.
DSV321SV-27.000MHz
Datasheet recommendation is 357LB3C027M0000 and described two spec.
![]()
On the other hand, DSV321SV&s specification doesn&t have APR.
①Frequency Tolerance: ±40x10^-6 Max
②Frequency Adjustment Range: ±100×10^-6 min. [Positive Slope]
Q1. Does ① or ② correspond to APR (Absolute pull range)?
Q2. The following E2E below seems to care about Phase noise by bandwidth when selecting.
DSV321SV has phase jitter defined, but I do not see how it relates to bandwidth bandwidth Phase noise.
It also stated that A higher APR should not cause an issue.
Can you please advise in general terms as well?
Best Regards,
ttd