This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: About the setting of LMX2594

Part Number: LMX2594

Could you please give me some advice?

When MASH_ORDER is "4" and fVCO>10000MHz, PFD_DLY_SET"6" is recommended.
When MASH_ORDER is "4", fVCO>10000MHz, and PFD_DLY_SET is "5", will the operation of the PLL IC become unstable?
If it becomes unstable, do you know what kind of unstable operation it will be?

Regards,
Akihiko Yokouchi/