Part Number: LMX2820
Hello
My understanding of the use of INSTCAL is that after applying the VCO band 3/4 transition patch I need to start a calibration at the low end of the VCO range (5650 MHz) and execute a normal calibration to build a full band look up table. What is the difference in operation between having bits zero and one of R1 (normal INSTCAL_EN, and INSTCAL_DBLR_EN)?
If i need to operate both in the non-doubled and doubled portion of the frequency range do I need to do a look up table generation for both?
thanks
Fred