Part Number: CDCM7005-SP
Other Parts Discussed in Thread: CDCM7005
Hello,
Datasheet 7.3 says VINPP min/max = 0.5V/1.3V.
However, note(2) says “VINPP minimum and maximum is required to maintain ac specifications; the actual device function tolerates at a minimum VINPP of 150 mV”. My customer is a bit confusing with those explanations.
Is the datasheet saying CDCM7005 is functional as a PLL when VINPP is more than equal to 150mVpp, but VINPP has to be 0.5Vpp to 1.3Vpp to meet all ac specifications? If yes, here, what are the exact ac specifications in the datasheet?
Best regards,
K.Hirano