Hello. I have a question.
We used under the following conditions:
HW_SW_CTRL = 0 (=Soft pin mode)
REFSEL = 1
(GPIO5, GPIO4, GPIO3, GPIO2, GPIO1, GPIO0) = (0, 1, Floating, Floating, 1, 1)
Chap.10.3.2.2 notes that when GPIO[3:2] are left floating, the hardware register default settings are loaded.
https://www.ti.com/document-viewer/ja-jp/LMK03318/datasheet/57-JAJSFA5E#SNAS6696874
In this case, when PRIREF is a single-ended clock and SECREF is GND, will the clock of OUT0_P and OUT0_N be something output?
Could you tell me if there is no or some clock output until clock output mutes before starting re-programming the desired register reprogramming via I2C?