This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVC1310-EVM: Saw Function as Output, Not Square Wave

Part Number: CDCLVC1310-EVM

I am using the CDCLVC1310-EVM. I am supplying 3.3V to both VDD and VDDO. I'm using the onboard 25MHz crystal oscillator to measure a square waveform, but am just getting a saw function instead. The output also varies from ~0.7V to ~2.5V.

The jumpers are as follows:

J40 shorted

J41 shorted

J38 shorted

J39 shorted

J43: shorted to VDD (2-3)

J42: shorted to GND (1-2)

How can I obtain a nice clean square wave?