This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04803: Regarding the multiple output clock frequencies from the clock synthesizer

Part Number: LMK04803
Other Parts Discussed in Thread: CDCM6208

Hello support team,

I have a clock generation requirement as below. 

Clock output 1: 74.25 MHz (LVDS 2.5 V)

Clock output 2: 125 MHz  (LVDS 2.5 V) 

Clock output 3: 25 MHz (LVDS 3.3 V)

Clock output 4: 33.33 MHz ( LVCMOS 1.8 V) 

All above frequencies can be possible to generate from single clock synthesizer with multiple outputs. As I have tried with the clock design tool but getting error of no solutions found.