Hi,
Kindly provide the current value of the following pins.
1.VccBUF
2.VccCP
3.VccDIG
4.VccMASH
5.VccVCO
6.VccVCO2
Regards,
Pavithra
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Kindly provide the current value of the following pins.
1.VccBUF
2.VccCP
3.VccDIG
4.VccMASH
5.VccVCO
6.VccVCO2
Regards,
Pavithra
Hi Pavithra,
The current consumption of the device will change depending on register configuration, VCO frequency, charge pump output, etc. For an arbitrary typical configuration with 2050MHz out and 100MHz in:
VccDIG: 63mA
VccCP: 26mA (charge pump set to 15mA effective gain)
VccBUF: 193mA (one output active - increase by about 92mA for two outputs active. Includes current through external pull-ups)
VccMASH: 18mA (3rd order, N=61.5)
VccVCO + VccVCO2: 130mA