Part Number: LM555
Other Parts Discussed in Thread: TLC555
Hi team,
My customer want a time delay device.
Clock signal :6.25MHz
delay: 30ns
Could you please recommend one?
Thanks,
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Brian,
None of the 555 timers will operate at this frequency. The TLC555 is the fastest device and ranges from 1.2 to 2.1 MHz. Propagation delays start to impact the 555 timers beyond 100 kHz operation. I am not sure a 555 timer device is the best option for this application. A microcontroller may be a better fit.
Best Regards,
Chris Featherstone