This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK1C1104: LMK1C1104DQFR

Part Number: LMK1C1104


To whom it may concern,

Does the continuous output current rating for the LMK1C1104DQFR refer to all outputs or each output?

Thank you,

D

  • Hi David,

    It is defined for each output. But running multiple outputs with that high current could results in high Tj values so we need to be careful about that. These are also absolute maximum values which means that exposure to these conditions is not recommended and it would result in reliability issues in long term.

    Best,

    Asim