Part Number: LMK04832
#1
I'm working on a customer board with a LMK04832.
We need single loop with PLL2 only with CLKin1 as PLL2 input.
I tried to program it and see no outputs at all - all outputs are enabled.
We don't use OSCin so no output at OSCout.
#2
The program codes are working for other type of customer board. This suggests that there may be something wrong with the hardware.
I measured the CPout1 and CPout2, CPout1 is 3.3V and CPout2 is 0V.
The RESET signal is LOW after power on.
CLKin_SEL[1:0] are '0'.
Any suggestions? Thank you.