Is somewhere the pin for “VBL” signal (video blanking),
I need to know exactly if the image has arrived.
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Evgeny,
If you are using Video Pattern Mode, then I suggest using Trigger Out 1 and/or Trigger Out 2. These are called out in the EVM guide.
The rising and falling edge can be delayed for these triggers - See Pattern Settings picture.
Trigger Out 1 marks out the exposure time (goes high and stays high) for each defined sequence that starts with a "Frame Change" (i.e. vsync).
Trigger Out 2 can be turned off or on per each sub-sequence and if set, marks the beginning of the subsequence with a pulse (it does not remain on for the whole sub-sequence). Notice that I turned off Trigger 2 for the second sub-sequence in the Pattern Design picture below.
NOTE: The Pattern Design picture below shows three 8-bit sub-sequences (based on G0-G7, R0-R7, and B0-B7). However, at 120 Hz input frame rate there is not enough time to show three 8-bit sub-sequences, only two.
Pattern Design:

Pattern Settings: