Part Number: LMX2581
Data sheet on Page 7 says OSCIn input voltage min=0.4Vpp, max=1.7Vpp.
Figure 12 and 13 show a much lower sensitivity, on the order of -27dBm.
Can you explain the differences in the data sheet?
Also, I'm using a CMOS TCXO and it appears the Hi-Z of the CMOS output is making this Ref OscIn input susceptible to interference from the PLL output. Every time I get close to a harmonic of 38.4M, I'm seeing spurs equal to the desired signal output. On the eval card, if I drive this Ref OscIn with an external 50 ohm Signal Gen, I don't get the spurs. I am using the LMX from 740 to 2500MHz.
I think I need a voltage divider to lower the termination on the Ref In but I need to know how low I can drop this level. Also, any suggestions for interfacing a CMOS output ref osc to the LMX2581 Ref Input?