Part Number: LMX2487E-EVM
Hi!
We want to generate a signal at 6.834 - 6.835 GHz. We are now using LMX2487E-EVM board and the VCO on the board is replaced to ROS-6840C-119+(www.minicircuits.com/.../ROS-6840C-119 .pdf) to provide 6.74-6.84 GHz VCO output range. The replaced VCO has same tuning voltage, supply voltage Vcc and a similar tuning sensitivity (85-100MHz/V) as the old VCO (100MHz/V). We expect the feedback parameters for the old VCO work for the new one. But the VCO output frequency is railed to the maximum or minimum of the VCO frequency range for both the old and the replaced VCO. The feedback is controlled by the TICS Pro software. Based on our current set up, what should we set up in the GUI below? Thanks a lot!