This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00338: Vcross doesn't meet PCIe gen5 spec

Part Number: LMK00338
Other Parts Discussed in Thread: LMK00334

 Hi team,

My customer wonders LMK00338 Vcross specification doesn't meet PCIe gen5 requirement.

Vcross is different from PCIe specification.

Looking at PCIe Gen4Refclk DC Specification and AC Timing Requirements  Table 8-16)or Gen5(Table 8-17) requirement, 

it is specified as : Vcross Absolute crossing point voltage     min +250mV    max +550mV.

The output specification is 90mV less than PCIe spec, so minimum value doesn't meet PCIe spec.

Why it doesn't meet PCIe spec while LMK00338 is supposed to support PCIe gen5? 

Best regards,

Itoh