Hi Team,
will CDCDB800 start and run correctly if it only has a pull up to VDD on the pin CKPWRGD_PD#? I did not find any timing requirement in the datasheet chapter Specifications.
Thanks.
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
will CDCDB800 start and run correctly if it only has a pull up to VDD on the pin CKPWRGD_PD#? I did not find any timing requirement in the datasheet chapter Specifications.
Thanks.
David
Hi David,
Recommended specification for CKPWRGD_PD# pin is to keep it low (< 0.5 V) until VDD reaches its VDD minimum value. VDD minimum value is 3.3 V - 5%. If you follow that requirement than there is no timing relation between VDD and CKPWRGD_PD#. Timing depends on your VDD ramp when it reaches VDD minimum valid value.
You can connect CLKPWGD_PD# pin to VDD through a pull up during ramp up and its a supported use case. There is an internal 10 - 40 us counter that makes sure everything is settled before anything is sent out. This counter turns on when digital supply reaches at a certain threshold so it could account for slow supply ramp cases.
Best,
Asim