This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2572LPEVM: Default output is not stable

Part Number: LMX2572LPEVM
Other Parts Discussed in Thread: LMX2572LP, LMX2572

Hello,

LMX2572LPEVM,Default output is not stable.

sometimes

・Default Configuration/Default Mode 2021-8-15→1500MHz

・Default Configuration/Test Mode→100MHz

some other time

・Default Configuration/Default Mode 2021-8-15→1800MHz

・Default Configuration/Test Mode→224MHz

The procedure is as follows.
(
Output value of stabilized power supply)
(1)PC ON、EVM ON(3.3V/34mA)

(2)Connect PC and EVM

(3)start the software TICS Pro EVM(3.3V/41mA)

(4)Select Device/PLL+VCO/LMX2572/LMX2572LP

sometimes

(5)Default Configuration/Default Mode 2021-8-15→1500MHz(3.3V/88mA)

(6)Default Configuration/Test Mode→100MHz(3.3V/95mA)

some other time

(5)Default Configuration/Default Mode 2021-8-15→1800MHz(3.3V/48mA)

(6)Default Configuration/Test Mode→224MHz(3.3V/62mA)